All the configuration parameters for an Advantys STB island cannot be written over the fieldbus via the application. Some specific parameters can be written to via the RTP (Run Time Parameters) functionality. Also a memory card (SIM card) can be used to store the configuration file, then on power up, the NIM will read its configuration from the card.
Released for:Schneider Electric Global