{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the 140NOC77100 Quantum Ethernet IP module scan a Allen Bradley Control Logix PLC?

Article available in these languages: Japanese

The 140NOC77100 cannot scan a Allen Bradley Control Logix PLC.
The reason for this is because of a proprietary way of peer to peer communication between Allen Bradley controllers.
They use Produce and Consume tags in order to synchronize information between PLCs and do not have an assembly object that the 140NOC77100 can scan.
Note: The 140NOC77100 can be an adapter to a Allen Bradley controller so the Control Logix PLC can scan the 140NOC77100.


Schneider Electric Global