Goals and Symptoms
Quantum 140CPU6xxx0 CPUs and M340 CPUs USB style programming cable connector description.
Facts and Changes
5-pin Mini B USB Type for use with M340 Processors
4-pin Mini B USB Type for use with Quantum 140CPU6xxx0 Processors
Causes and Fixes
The M340 USB programming cables are BMXXCAUSBH018 (1.8m) and BMXXCAUSBH045 (4.5m) which have a USB Type mini B 5-pin connector. The Quantum USB programming cable is UNYXCAUSB033 (3.3m) which has a USB Type mini B 4-pin connector.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global