{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What does 'HMI R/W mode' on the EcoStruxure Control Expert status bar mean?

Issue
HMI access rights

Product Line
EcoStruxure Control Expert
Unity Pro

Resolution
This indicates the HMI access rights. A project (application) can have different modes:

1/ HMI R/W mode - HUMAN_MACHINE_INTERFACE Read/Write mode is the default mode when opening a project.

2/ HMI R/O mode - Read only mode is active when:.
- a project is opened in Read Only mode by checking the option 'Open the project in read-only mode' in
the Open file window.
- opening a project that was previously opened in Write mode using Pserver (2nd session of Unity).
A popup window alerts the user when opening the project. This mode does not allow saving of the project.
The user will be asked if he/she wants to switch to the currently opened session of Unity Pro.

Schneider Electric Global