{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the level of protection to the mechanical shocks of the XB5S: IK index.

Goals and Symptoms

What is the level of protection to the mechanical shocks of the XB5S: IK index.

Facts and Changes

XB5S
Mechanical shocks
IK

Causes and Fixes

The XB5S is IK03.


Legacy KB System (APS) Data: RESL200556 V1.0, Originally authored by LaBe on 11/23/2009, Last Edited by LaBe on 11/23/2009
Related ranges: Harmony XB5S