{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the system requirements for Concept 2.6 SR6?

1. System requirements for Concept 2.6 SR6:
- x86-based personal computer (Pentium platform recommended)
- Win98, Win2000, or WinNT 4.0 SP3 or higher (Y2K compatibility requires SP5 ), WinXP Pro or Windows Vista Business 32 Bit
- Win95 is no longer qualified. Win3.1x is no longer supported.
- 24 MB application RAM (or higher)
- CD-Rom drive
- 150 MB hard disk space
- VGA graphics adapter and screen (minimum resolution: 800x600)
- Microsoft compatible mouse

Concept 2.6 SR6 does not support Windows 7 Professional (32). You would need to upgrade to Concept 2.6 SR7 to run on Windows 7 (32)



Schneider Electric Global