UPDATE 3/29/13 (doc revision 20130329)
Firmware History for version 6.0 - excel format
UPDATE 12/21/2012
zip file contains pdf's:
1. Firmware History for version 5.6.
2. Command 15 behavior
3. Sub-Function 16 behavior
UPDATE 9/10/2012
zip file contains pdf's:
1. Firmware History for version 5.5.
2. Command 15 behavior
3. Sub-Function 16 behavior
UPDATE 12/15/2011
zip file contains pdf's:
1. Firmware History for version 5.1.
2. Command 15 behavior
3. Sub-Function 16 behavior
UPDATE 7/7/2011
zip file contains pdf's:
1. Firmware History for version 5.0.
2. Command 15 behavior
3. Sub-Function 16 behavior
UPDATE 12/22/10:
1. Release of version 4.8.
2. Added new title to section of Release Notes version 4.7; The NOE is incorrectly assigned an address of 'configured IP+1' instead of the 'configured IP' in a standalone 140CPU6716x.
Legacy KB System (APS) Data: RESL202381 V8.0, Originally authored by DaDz on 05/29/2010, Last Edited by DaDz on 03/30/2013
Related ranges: Modicon Quantum