Issue
This Resolution contains the Release Notes for the BMXNOC0401 firmware version 2.03.
The attached document describes the Issues, Results, and Customer Actions of the changes to firmware version 2.03, 2.02, 2.01, and 1.02.
Product Line
M340
BMXNOC0401
Environment
Resolution
Refer to the attached document for the complete details.
Attachments
NOC0401 Exec v2.03 Release Notes.zip
- Updated 1/11/13
Release of version 2.03 (New Format) - Updated 1/11/13
Release of version 2.02 - Created 2/15/12
Release of version 1.02
Released for:Schneider Electric Global