{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
140NOE77111 Exec Version 5.5 Release Notes

Issue
This Resolution contains the Release Notes for the 140NOE77111 Exec firmware version 5.5.

The attached document describes the Issues, Results, and Customer Actions of the changes to Exec versions 5.5, 5.1, 5.0, 4.8, and 4.7


Product Line
140NOE77111


Environment


Resolution
Refer to the attached document for the complete details.

Attachments
Release Notes for the NOE77111 Exec v5.6 will be available by Jan 4, 2013.

NOE77111 Exec v5.5 Release Notes.zip

  • UPDATE 9/10/2012
    zip file contains pdf's:
    1. Release Notes for version 5.5.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 12/15/2011
    zip file contains pdf's:
    1. Release Notes for version 5.1.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 7/7/2011
    zip file contains pdf's:
    1. Release Notes for version 5.0.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 12/22/10:
    1. Release of version 4.8.
    2. Added new title to section of Release Notes version 4.7; The NOE is incorrectly assigned an address of 'configured IP+1' instead of the 'configured IP' in a standalone 140CPU6716x.

Schneider Electric Global

Attachment(s)
NOE77111_v5.5_Release_Notes.zip [126.22 KB]