Up to eight load cells can be connected to the weighing module. If more than one load cell is used, then the cells must first be connected to a load cell junction box, then to the 15 pin sub D connector on the Momentum base.
Released for:Schneider Electric Global