Issue:
What is the time base used for the INT_TO_REAL function Control Expert (formally Unity Pro)?
Product line:
Unity Momentum, Quantum, M340, M580
Environment:
Ecostruxure Control Expert (formally Unity Pro).
Cause:
To determine the time base for setting up the block.
Resolution:
The Unity Pro INT_TO_TIME EFB time base is in milliseconds. An example would be a value of 25,000 is 25 seconds - this is the same as T#25s for data type TIME.
Released for:Schneider Electric Global