Issue
How to add a '.dat' formatted loadable t 'ProWORX NxT'
Product Line
'ProWORX NxT'
Environment
Windows 7, 10
Resolution
The following steps can be used to add a custom loadable (e.g. EUCA loadable, etc.) that is in the form of '.dat' to
a '.ProWORX NxT' project.
- Click on 'Configuration\Configuration'.
- Click on the 'Loadable Library' tab.
- Select 'Modicon' in the 'Source of Loadables' section of the 'Loadable Library' tab.
- Click on Browse:
- Select the 'EUCA-8.dat'.
- Click on OK
- Click on Transfer.
- Browse for the 'PROWORX.USL'.
- Click on OK.
- Click on the "User Loadables' tab.
- Select the 'EUCA' loadable to select it..
- Click on the 'Load' button to add the loadable into the project database..
- Click on 'OK' to close the 'Controller Configuration' window.
Released for:Schneider Electric Global