{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ION Enterprise 5.0 - Installing a Remote SQL Server Instance and Separating the Databases from the Application

Product Line:
ION Enterprise 5.0

Environment:
Remote SQL Server

Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

The attached document provides instructions for separating the SQL databases from the ION Enterprise 5.0 application and installing them on a separate server. Please note that this information and the attached scripts are being provided "as is" as this version of ION Enterprise is no longer officially supported.

Schneider Electric Global

Attachment(s)
Installing_Remote_SQL_Server_Instance_and_Separating_the_ION_Enterprise_DBs_from_the_Application.pdf [1.09 MB]
CreateIONlogin.sql [727 Bytes]
Folder.bat [871 Bytes]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.