{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I order a CVMT for a CM4000T separately?
Issue
The CM4000T is shipped with one CVMT (Current Voltage Module). Is the CVMT sold independently of the circuit monitor in the case that a replacement is needed?

Product Line
CM4000T

Environment
Product Availability

Resolution
Yes, the Current/Voltage Module can be ordered separately.

The CVMT supports high speed transient detection.

Note: Previously, there was another type of Current Voltage Module. However, now the CVM42 is obsolete along with the CM4250. The CVM42 supported an anti-aliasing filter and was compatible with the CM4000 and the CM4250.

Schneider Electric Global