{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I set the address and baud rate on a CM100/200 series meter?

Product Line
CM100/200 series meter

Environment
Communication Setup

Resolution
Follow the steps below to set the address and baud rate.

  1. Disconnect control power from the unit
  2. Set the 2 rotary selector dials to the correct setting for the baud rate (97=9600).
Switch SettingBaud Rate
941200
952400
964800
979600(default)
9819.2K
  1. Restore power
  2. Wait 5 seconds, disconnect power again
  3. Set the 2 dials to the desired address (Range includes 1 to 32)
  4. Restore power.

Schneider Electric Global