{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can One Remote Display be Used for Multiple Meters for the CM4000 or CM3000 or PM800 or PM5000 or PM8000
Issue
Viewing multiple devices on one Remote display screen

Product Line
CM3000
CM4000
PM800
PM5000
PM8000

Environment
Hardware Capabilities

Cause
The remote display is tied to only one meter

Resolution
The remote display is intended for use with a single meter. Other standard operator interfaces, such as Magellis, that support Modbus and RS-485 can be used to display data from multiple meters using one of the comm ports on the meter.