{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can transient detection be added to an existing Series 4000 Circuit Monitor?

Issue
Is it possible to upgrade a CM4000 so it has transient detection

Product Line
CM4000
CM4000T

Environment
Field Retrofit
Hardware upgrades

Cause
By default the CM4000 does not have transient detection.

Resolution
Yes. The difference between a standard CM4000 and a CM4000T is firmware and removable module called a Current Voltage Module (CVM on the CM4000, CVMT on the CM4000T). The CVMT can be purchased separately to upgrade a CM4000 to a CM4000T. The CVMT kit includes all of the hardware, software, and instructions necessary to upgrade a standard CM4000 to a CM4000T. The CVMT kit includes the following: CVMT (Current Voltage Module for transient detection), CVMT Installation Instructions, Hardware kit (spade lugs), CM4000 Firmware upgrade CD (Includes circuit monitor firmware and the softwareDLF-3000 used to download the firmware), CM4000T instruction bulletin, CM4000 instruction bulletin (English, French, Spanish), CM4000 technical library CD, System Manager Software upgrade CD (if necessary).

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.