Issue
What are the screw size and wire sizes for the CT and PT terminal connections
Product Line
CM4000
CM4250
CM4000T
Environment
Hardware Specifications
Resolution
The terminal screws are 4mm with a 0.7 pitch. Each meter is supplied with spade lugs that accommodate 10-12 AWG wire.
What are the screw size and wire sizes for the CT and PT terminal connections
Product Line
CM4000
CM4250
CM4000T
Environment
Hardware Specifications
Resolution
The terminal screws are 4mm with a 0.7 pitch. Each meter is supplied with spade lugs that accommodate 10-12 AWG wire.
Released for:Schneider Electric Global