{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to use BCM CT Strips with BCPM?

Issue
Is it possible to use BCM CT Strips with BCPM?

Product Line
BCPM
BCM

Environment
CT Selection

Resolution
It is NOT possible to use BCM strips with a BCPM. In order to maintain the specified accuracy it is important to only use the CT strips that came with the unit. Matching the serial numbers of the board and CT strips is one of the steps in the installation of the BCPM.

Schneider Electric Global