{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to see RMS value on Vista waveform?

Issue
In WebReach I can see the waveform and its RMS value. Is this possible in Vista?

Product Line
ION Enterprise, SPM, PME

Environment
Vista

Cause
Unfortunately, you CANNOT plot this RMS value in Vista. However, the data is still available.

Resolution
Right click on the background of your Vista waveform plot and select "Graph Options". Check the box: "Show calculations". RMS is included in these calculations. You can move Cursors 1 and 2 by dragging them from the left and right edges of the graph, calculations will update in real time



For PME7.2.2 and previous version, extra configuration is required to make PME work with a 50 HZ system.  Details please refer to KB How do I configure WebReach for a 50 Hz system?

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.