Issue
Clarify the dimension of ION 8650 meter switchboard (285 x 228 x 163) on page-4 under mechanical characteristics of ION8650 datasheet. The (285 x 228 x 163) dimensions are not mentioned on page-8 of ION8650 datasheet.
Product Line
ION8650 Switchboard
Environment
Mechanical Dimensions
Cause
The datasheet showing the meter dimensions is misleading
Resolution
The correct dimensions are like those in the mechanical drawing: 226 mm high x 147 mm wide x 189 mm deep. The required cut-out will be, as on page 3, 149 mm wide x 230 mm tall.
Note: the mounting bolts are size 10-32.
Released for:Schneider Electric Global