Product Line
ION Meters
Environment
FTP
Resolution
To connect to a meter using an FTP connection, the username and password can be included in the FTP connection string. The examples below demonstrate how to use the connection string to connect to a meter with an IP address of 123.45.6.78 using Windows Explorer:
Example 1: Standard Security and the default front panel password of 0:
ftp://0:0@123.45.6.78
Example 2: Advanced Security with user1 and password of 12:
ftp://user1:12@123.45.6.78
Released for: Schneider Electric Global