{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is FACT (factory) protocol for ION 6200 or ION7650/7550 Meters?

Issue
What does FACt mean under protocols

Product Line
ION6200
ION7550
ION7650

Environment
Hardware protocols and specification

Resolution
Factory protocol is a terminal-like interface used at the factory for initial configuration and calibration during production. For most circumstances, this protocol should not be used once the meter is installed.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: