Issue
When you attempt to search for a System page in Graphics Builder from File>Open, you can not locate them.
Product
Powerlogic Scada 7.1/7.2
PowerSCADA Expert 7.3/7.4/ 8.x
EcoStruxure™ Power SCADA Operation 8.2
Environment
Graphics Builder pages search function
Cause
System pages are prefixed with an exclamation mark (!) and are not normally visible when searching for Graphics pages.
Resolution
In order to view these pages you need to ensure that you select 'List System Pages'. To set this property, navigate to Tools>Options in Graphics Builder and ensure that 'List System Pages' is checked.
The following video demonstrates this procedure:
Released for:Schneider Electric Global