Issue
Would like to know fuse class for fuses included in the energy meter fuse packs
Product Line
EMFP1
EMFP2
EMFP3
Environment
Installation
Resolution
The replacement fuses for the voltage fuse pack with the Enercept Meter or Energy Meter are 1/2 AMP Cooper, Bussmann, FNQ-R-1/2, CC-Tron, Class CC, Slow Blow.
Released for:Schneider Electric Global