{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are communication cards interchangeable / compatible between ION 7500, 7600, 7550 and 7650 meters?
Issue:
A user wants to take a communication card from an ION 7500, 7600, 7550, or 7650 meter and use it in another ION 7500, 7600, 7550, or 7650 meter. They need to know if there are compatibility issues.

Product Line:
ION7500, ION 7600, ION 7550, ION 7650

Environment:
Communications

Cause:
A user would like to re-use existing hardware.

Resolution:
A communication card from a 7500, 7600, 7550, or 7650 will work in any of the four meters.

For example, a communications card from a 7500 will work in a 7650 and vice versa.

******************************************************************CAUTION*****************************************************************
Always power down the meters and disconnect voltage and current inputs before removing or inserting a communication card.

Schneider Electric Global