Product Line
Enercept Meter
Environment
Voltage Mode Setup
Resolution
The factory default for the meter is a system type 40, but the following options are valid:
20 = Single Phase, 2 Wire
21 = Single Phase, 3 Wire
30 = Three Phase Delta
40 = Three Phase Wye
Write one of these values to the Single Holding Register 36.
Reference the video in FA180037 for information on how to write to registers.
Released for:Schneider Electric Global