{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the pulse width on digital output for a 6200 meter?

Issue:

Pulse width output

Product Line:

ION6200

Environment:
ION 6200

Cause:
Time Constant, kT, is the number of units (kWh,kVah,kVARh) per output transition.

Resolution:
The digital output uses KY pulsing. This means that the relay changes from open to closed or from closed to open whenever kT units have been measured (20 transitions/second maximum).