Product Line
ION6200
Environment
Front display of ION6200
Resolution
For non-revenue sealed meters running firmware version v205 and later, the energy (kWh), peak current, and peak demand registers can be reset from the front panel.
ION6200
Environment
Front display of ION6200
Resolution
For non-revenue sealed meters running firmware version v205 and later, the energy (kWh), peak current, and peak demand registers can be reset from the front panel.
- Press and hold the round button until Curr, PWr, and EnEr are displayed in the three lines
- Curr: Current Maximum Demand Reset
- PWr: Power Maximum Demand Reset
- EnEr: Energy Reset
- Select the parameter to be reset and press the round button
- Confirm the reset and enter the front panel password
- Press and hold the round button to exit
Released for:Schneider Electric Global