{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Clicking on Numeric control object on the network diagram does not work in webreach.

Goals and Symptoms

A user has numeric control on their network diagram, and the action is set to open another diagram in the same folder, say map.dgm. All works fine in Vista, but in webreach, clicking on the control opens a blank page, and not the map.dgm.

Causes and Fixes

Reseting the IIS will resolve the problem.
Steps to reset the IIS:

  1. Open a DOS window
  2. Type <iisreset> without the brackets




Last Revised: November 8, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189048 V1.0, Originally authored by KBAdPM on 11/09/2007, Last Edited by KBAdPM on 11/09/2007
Related ranges: ION Enterprise V5.5

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.