{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the accuracy of the phase angle measurement on the ION 7650?

The Power Harmonics Module has phase angle accuracy within (±0.5º x harmonic number); hence, the deviation may increase with higher harmonics. In addition, the Power Harmonics Module is limited to a 2 second update rate since the module is driven from the FFT modules, which have a 2 second update time.

Last Revised: December 3, 2007
Applies To: ION 7650
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189894 V1.0, Originally authored by KBAdPM on 12/03/2007, Last Edited by KBAdPM on 12/03/2007
Related ranges: ION7550/ION7650

Schneider Electric Global