{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I run ION and Modbus protocol on the same serial chain

Issue
In many situations, PM8000 series meters were purchased as a direct replacement to the legacy PM800 series meter.

Product Line
Power Monitoring Expert
ION9000 & ION9000T
PM8000
ION7400

Environment
Device Communications

Cause
Because the PM8000 meter was designated as the direct replacement for the PM800 series meter, ION over Modbus was designed and implemented into the PM8000, the ION7400, and the ION9000 series meters.

Resolution
For more information about implementing the "ION over Modbus" solution please look to article FA331587

Schneider Electric Global