{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can we use Aluminium cable ?

Goals and Symptoms

Can we use Aluminium cable ?

Facts and Changes

AB1VVN7035U

Causes and Fixes

It is not recommended to used our terminal block type AB1VVN with alu-cable because it is necessary to check regularly the tightening couple.
You can used alu cable but it is necessary to respect some rules.
1. After denude alu-cable, clean the alu cable and treat it with a grease in order to avert the oxidation.
2. alu cable must be tighten with a couple higher than the moninal tightening couple. ( 65%, 10Nm)
3. It is necessary to tighten again the cable 15 days after the montage.
Then, check the tightening couple 1 or 2 times by years ( depend on the applicaion )
4. The maximum current must be 60% of the nominal current.


Legacy KB System (APS) Data: RESL198038 V1.0, Originally authored by LaBe on 03/14/2009, Last Edited by LaBe on 03/14/2009
Related ranges: AB1, DB6

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.