Issue
User would like to use ION Setup to connect to an ION6200 meter in single device mode
Product Line
ION6200
Environment
ION Setup
Resolution
No, ION Setup cannot connect to an ION6200 in Single Device Mode. Network Mode is required.
- Right click > Insert Item > Group
- Select the created group
- Right click >Insert Item > Site
- Configure the Site (Serial/Ethernet)
- Right click > Insert Item > Meter
- Configure the ION6200 meter
- Click OK
You should now be able to double click the meter and access its modules.
Released for:Schneider Electric Global