{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
You do not have authority to make configuration changes to this node diagram" error message appears in Designer

Issue
The following error message appears when trying to add, modify, or delete a module for a meter, or the VIP content in designer.


Product Line
ION Enterprise 5.6/6.0
Struxureware Power Monitoring 7.0
Power Monitoring Expert 7.2/8.0/8.1

Cause
Node diagram for the device might be read only, and the customer might not be log in the system as an Administrator

Environment
ION Enterprise 5.6/6.0
Struxureware Power Monitoring 7.0
Power Monitoring Expert 7.2/8.0


Cause
Rights and permissions of the folder might not be setup properly for the user

Resolution
Try both workarounds

1) Close Designer and try to reopen it by Right clicking on it. Then, select "Run as an Administrator"

2) To resolve this error make sure that the node diagram for the device is not read only:
a) - Browse to ...\ION Enterprise\config\diagrams\nd if you are using ION Enterprise5.6/6.0 or Struxureware Power Monitoring 7.0
- Browse to ...\Power Monitoring Expert\config\diagrams\nd if you are using Power Monitoring Expert 7.2/8.0
b) Find the device that is having the issue.
c) Right click and go to properties.
d) Make sure the file is not set to read only on the general tab.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.