{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there quick method to check the SQL Server’s version and edition instead of using a SQL query script?

Yes, there is another quick way to check the version number and the corresponding product edition from the SQL Server Management Studio or SQL Server Management Studio Express indeed. But please note that using the SQL query script is the official way recommended from Microsoft to identify your current Microsoft SQL Server version number and the corresponding product or service pack level.

    1. As the figure shown below, in the SQL Server Management Studio or SQL Server Management Studio Express, right-click on the Server (marked with (i.) in the figure) then select the Properties from the list to open up a Server Properties Window.
    2. The Product (marked with (iii.) in the figure) and Version (marked with (iv.) in the figure) would be found in the General page (marked with (ii.) in the figure) of the Server Properties Window.
    3. From the above, this SQL Server could be identifying as Microsoft SQL Server Standard Edition from Product and its version is 9.00.4005.00, i.e. SQL Server 2005 Service Pack 3.

More Information
    • Possible Product edition:
          • Microsoft SQL Server Standard Edition or
          • Microsoft SQL Server Enterprise Evaluation Edition or
          • Microsoft SQL Server Express Edition or
          • etc

      Existing Version number:
      ReleaseSQL Server 2000SQL Server 2005SQL Server 2008
      SQL Server RTM8.00.1xxx.009.00.1xxx.0010.00.1xxx.00
      SQL Server Service Pack 18.00.2xxx.009.00.2xxx.0010.00.2xxx.00
      SQL Server Service Pack 28.00.3xxx.009.00.3xxx.0010.00.3xxx.00
      SQL Server Service Pack 38.00.4xxx.009.00.4xxx.0010.00.4xxx.00

Related Articles:

Identifying SQL Server 2000 Service Pack version from Diagnostics (.cab) file

Checking SQL Server 2000 or MSDE Version and Service Pack Level

What version of SQL Server is used with the different versions of ION Enterprise?


Legacy KB System (APS) Data: RESL201100 V1.0, Originally authored by KBAdPM on 01/22/2010, Last Edited by KBAdPM on 01/22/2010
Related ranges: ION Enterprise V5.5, ION Enterprise V6.0, ION Enterprise V5.6

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.