Release Notice
Summary
The sliding window demand modules in the "ION Revenue Test Framework" cannot be reset with a push-button. The "Demand Reset" button will reset the values but the period will not reset.
Goals and Symptoms
Symptoms
The period of the sliding window demand modules in the ION Revenue Test Framework cannot be reset. This causes issues while testing. The period of the sliding windows are in sync with the system clock on the meter and will only reset on certain times, which means the test can only start at certain times as well. For example, if the period of the Sliding Window Demand modules are set to 15 minutes, the periods will only reset at the 00, 15, 30, and 45 minute mark.
Causes and Fixes
Work Around
Make the following changes in the ION Revenue Test Framework
1) Place a new pulse merge module. Pulse in 1 input should be connected to Test Dmd Rset of the Test Dmd Rset module. Pulse in 2 input should be connected to CNV1 On Pulse output of the Test Mode Rset module.2) Place a oneshot timer module. The sync input of this module should be linked to the Pulse Out of the Pulse Merge module which was placed in step 1.
3) The Trigger output of the One Shot timer (placed in step 2) should be connect to the sync input of both KW sd del T and KW sd rec T
* red box indicates added modules
Resolution
Download the appropriate corrected template to the device.
Corrected framework for affected meters
8600A_V330_FAC-35S_V3.3.0.0.4.fwn
8600A_V330_FAC-35S-PQ_V3.3.0.0.5.fwn
8600A_V330_FAC_V3.3.0.0.4.fwn
8600A_V330_FAC-PQ_V3.3.0.0.5.fwn
8600B_V330_FAC-35S_V3.3.0.0.4.fwn
8600B_V330_FAC_V3.3.0.0.4.fwn
8600C_V330_FAC-35S_V3.3.0.0.4.fwn
8600C_V330_FAC_V3.3.0.0.4.fwn
Attachments
(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/a199b668dcaa9454c12577160010c02b/fl_block_5/0.1A60?OpenElement&FieldElemFormat=gif)
Date Created: April 19, 2010
Last Revised: April 30, 2010
Public
Original Author: TO
All content © 1992-2010 Schneider Electric
Legacy KB System (APS) Data: RESL202153 V1.0, Originally authored by MiNe on 05/01/2010, Last Edited by MiNe on 05/01/2010
Related ranges: ION8600
Released for:Schneider Electric Global