{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does Service Release 1 Need to be Installed Before Running Service Release 2 for PowerLogic SCADA v7.10 r01?

No. PowerLogic SCADA Service Release 1 (PLS SR1) does not need to be individually run before installing Service Release 2 (SR2).
The SR2 install will detect that SR1 has not been previously installed and will install it automatically.




Keywords: PLSCADA, PL SCADA, service pack, r01.1, r01.2


Legacy KB System (APS) Data: RESL203436 V1.0, Originally authored by AnVa on 09/15/2010, Last Edited by AnVa on 09/15/2010
Related ranges: PowerLogic SCADA 7.1

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.