{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to create custom device types in the EGX300?

Issue
Is it possible to create custom device types in the EGX300?

Product Line
EGX300

Environment
EGX300 Real Time Monitoring

Resolution
The Custom Device Type Generator (CDTG) is a server-based application used for adding basic support for third party devices into EGX300. The CDTG provides an interface for collecting device information needed to support a custom or third party device. This information is then stored on the EGX in a custom device configuration file (*.dtc). From this file, the application will create and install the files needed by the EGX300 to support the new custom device.

The attached document describes the process of creating a custom device driver in the EGX300, so that real time readings can be viewed in the monitoring page.

Schneider Electric Global

Attachment(s)
Custom_Device_Type_Generator_KB.pdf [259.04 KB]