{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
DNPR (Providing DNP3 Support) Driver is Not Selectable in I/O Device Protocol Field in PowerLogic SCADA v7.20

The documentation for PowerLogic SCADA (PLS) v7.20 states that DNP3 is a natively supported protocol. However, the user may find that DNP3 and/or DNPR are not available to select after installing.
This is most likely because the DNPR driver is not selected to be installed by default. The user must manually check to install this driver.


Legacy KB System (APS) Data: RESL207955 V1.0, Originally authored by AnVa on 04/21/2012, Last Edited by AnVa on 04/21/2012
Related ranges: PowerSCADA Expert 7.2, PowerLogic SCADA 7.1

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.