The part number for SER is9789SER. The part number for ENM is 9789ENM.
Notes:
- A PowerSCADA Expert system with redundant alarm servers requires 2 ENM licenses (part number x 2).
- ENM supersedes previous paging solutions: Active Paging Module, Event Notification Solution
For more information about these PRODUCTS, please contact a local Schneider Electric sales representative.
Keywords: PLSER, PLSSER, PowerLogic SER, recording, 7.1, 7.2, 7.3, 7.4, 7.5, Active Pager Module, APM, ENS, 6.0, 6.1, 6.2, 6.3, 6.4, 6.5, 6.6, 7.0, PLAPM, PowerLogic SCADA, PLS
Legacy KB System (APS) Data: RESL208781 V1.0, Originally authored by AnVa on 08/03/2012, Last Edited by AnVa on 08/03/2012
Related ranges: SMS Add-on, Paging Module, Sequence of Events Recorder (SER)
Released for:Schneider Electric Global