{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number for the replacement battery on a ION7550 or ION7650? Can this be ordered?

Issue
What is the part number for the a battery replacement on the ION7X50

Product Line
ION7650
ION7550
ION7600
ION7500

Environment
Product Selection

Resolution
Schneider Electric no longer sells replacement batteries for the ION 7550 and ION 7650 because the batteries are now soldered to the board. For older versions of the meter, the battery can be replaced with a "Tadiran Model: TL-5276/W or equivalent". Please follow the attached document for battery replacement instructions.

Schneider Electric Global

Attachment(s)
ION7550_ION7650_Battery_Replacement_Instructions.pdf [858.41 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.