Issue
Using a Modbus tester (Video: What is Modbus Tester and how do I use it?) to read 'Mod10' type registers will return a series of registers that need to be converted in order to find the decimal value. For example most CM4000 energy related registers are Mod10 type and only differ in 'size' (number of registers); some are four registers and some are three. This article gives the conversion formulas for three and four size registers and then uses a tester to read a CM4000 register for testing and verification.
Product Line
PM800 series meters
CM3000 series meters
CM4000 series meters
Environment
Reading Energy values via Modbus register reads on Powerlogic meters
Cause
The energy values on many Powerlogic meters are stored in several 16-bit registers in a Modulo 10k format.
Resolution
Depending on the 'size', use one of the following formulas:
1. 48-bit signed value returned in three consecutive 16-bit registers where R3 is the last register and R1 is the first register. Each registers range is -9,999 to +9,999:
R3*10,000^2 + R2*10,000 + R1
2. 48-bit unsigned value returned in three consecutive 16-bit registers where R3 is the last register and R1 is the first register. Each registers range is 0 to +9,999:
R3*10,000^2 + R2*10,000 + R1
3. 64-bit signed value returned in four consecutive 16-bit registers, where R4 is the last register and R1 is the first register. Each registers range is -9,999 to +9,999:
R4*10,000^3 + R3*10,000^2 + R2*10,000 + R1
4. 64-bit unsigned value returned in four consecutive 16-bit registers, where R4 is the last register and R1 is the first register. Each registers range is 0 to +9,999:
R4*10,000^3 + R3*10,000^2 + R2*10,000 + R1
Note that the same formula is used whether register is signed or unsigned
Example
Referring to Modbus map of CM4000, register 4x1716 which corresponds to Total Real Energy (signed/absolute) is read; note that this register has a size of four, meaning four consecutive registers of type Mod10 should be read and converted.
Using formula 3 the conversion results in:
0 * 10,000^3 + 45 * 10,000^2 + 9300 * 10,000 + 8131 = 4,593,008,131
Which matches the value read by ION Setup:
Released for: Schneider Electric Global