undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What USB-to-RS485 or USB-to-RS232 converters should I use to communicate with ION or PowerLogic meters?
Issue
A user may want to use a software program to communicate to a PowerLogic or ION meter when ethernet is not an option.

Product Line
ION and PowerLogic meters.

Environment
ION Setup, Modbus Tester, DLF-3000

Cause
Many meters do not have ethernet as an option, or the ethernet option was not ordered, or the ethernet port is in use and cannot be disturbed.

Resolution
The commonly recommended USB-to-RS485  converter is the USOPTL4 by B&B Electronics. It works well with ION and PowerLogic products that have a 2 wire or 4 wire RS485 port.

The commonly recommended USB-to-RS232 converter is the USO9ML2 by B&B Electronics. It works well with ION and PowerLogic products that have either a DB9 serial port or dedicated terminals for for RS232..

Attached is the quick start guides which is very helpful for wiring questions.  Pay special attention to the “4 Wire Set-up”/ “2 Wire Set-up” to help eliminate wiring errors.

To find out which meters support RS 232 and which support RS 485, many meter's basic features are outlined in a chart on page 7 and 8 (or pages 12-14 as numbered in the document) in the attached file below titled "Product_Range_Overview.pdf".

Schneider Electric Global

Attachment(s)
USOPTL4_quick_guide.pdf [585.86 KB]
USO9ML2_quick_guide.pdf [319.36 KB]
Product_Range_Overview.pdf [2.22 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.