Product line
Power Monitoring Expert 8.x
Power Monitoring Expert 7.2.x
StruxureWare Power Monitoring 7.0.x
ION Enterprise 6.0.x
Environment
Operating System Compatibility
Cause
A user would like to know if Windows 7 Ultimate is a supported operating system for the PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x software platforms.
Resolution
Both the 32 and 64 bit versions of Windows 7 Ultimate are supported for PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x installations.
Power Monitoring Expert 8.x
Power Monitoring Expert 7.2.x
StruxureWare Power Monitoring 7.0.x
ION Enterprise 6.0.x
Environment
Operating System Compatibility
Cause
A user would like to know if Windows 7 Ultimate is a supported operating system for the PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x software platforms.
Resolution
Both the 32 and 64 bit versions of Windows 7 Ultimate are supported for PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x installations.
Released for:Schneider Electric Global