Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
Does the I/O Expander module for an ION 8600 work with an ION 8500?

Issue
The I/O Expander module for the ION 8600 is compatible with the ION 8300, 8400, and 8500 series power meters as long as the meter's firmware is at an appropriate version.

Product Line

The required firmware versions are listed in the table below.

I/O PortsION 8300, ION 8400,
ION 8500 Firmware Version
ION 8600
Firmware Version
Digital Inputsv203 and higherv310 and higher
Digital Outputsv203 and higherv310 and higher
Analog Outputsv205 and higherv310 and higher


The part numbers for the IO Expander module options are listed below.

IO Module Options

The I/O Expander module connects to the meter utilizing the 24-pin Molex connector, and break out both the I/O options and the serial communication options (COM1 and COM2/COM4 depending on meter).

Legacy KB System (APS) Data: RESL212830 V1.0, Originally authored by LaLo on 10/22/2013, Last Edited by LaLo on 10/22/2013
Related ranges: ION8500, ION8600

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings