Only one exchange can be made at a time: if the module is waiting for a response from the device, it cannot send a request. TCP requests
are suspended on the network (a maximum of 128 pending requests).
Released for:Schneider Electric Global


{}
Only one exchange can be made at a time: if the module is waiting for a response from the device, it cannot send a request. TCP requests
are suspended on the network (a maximum of 128 pending requests).