{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the purpose of the 170XTS04200 Modbus RS485 terminating RJ45 shunt plugs?

The 170XTS04200 Shunt plugs are used with the RS485 connector (RJ45 base) at one end of a two-wire cable network. The plug is used at the last device on the network.