{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Unable to read per phase Power Factors on a 3 Wire System

Issue
Unable to read per phase power factors

Product Line
CM100
CM200
CM2000
CM4000
Enercept

Environment
Power Factor

Cause
No neutral

Resolution
Meters with a 3-phase 3-wire configuration are unable to monitor per phase power factors because they do not have a true neutral to reference. When reading per phase power factors for a series CM100/200 the result returned is the value for the total system power factor. On the series 2000 Circuit Monitor, the readings are N/A for individual phase power factor.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.