{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to read CM2000 registers from Wonderware software using an ECM
Product Line
CM2000
ECM

Environment
Modbus Register reads

Resolution
In order to read the CM2000 registers through an ECM module, Wonderware requires 30,000 added to the register number. Example: register 1003 in the CM2 would be read as 31003 in Wonderware.

Schneider Electric Global